Other Parts Discussed in Thread: CD14538B
Hi,
We use a CD14538BPW to have a 1s trigger.
With the formula T=CxRx, I have Cx=10uF et Rx=100K.
At 20°C the pulse is 1s, but at 70°C the pulse is near 500ms.
The Temperature operation range of CD14538B is -55 to +125 so we are in the spec.
Do you have an idea to explain our problem?
Arthur