This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCLVC1104 and SN74AUP1G79 latch up?



Hi,

I have a lvcmos clock buffer driving an D-Flip flop, and lvcmos buffer listed above. Once the boards came back assembled the clock line signal was attenuated and offset. At first I thought the oscillator was bad, but after pulling off the oscillator from the board, I measured a DC value of 3.3 V on the clock line. Either the flip flop or the buffer is bad. This happened on multiple boards. Is this a latch-up issue? I have used this design in the past with a slightly different layout. Any ideas?

FYI. The clock line is not pulled down or ac coupled to the oscillator. From my reading I should not have to with LVCMOS logic.

Thanks

Jordan