This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0108PWR question

Hi,

I'm using LSF0108PWR with VREFA at 1.8V and VREFB at 3.3V with 1K pull up for all the 8 input and output channels.

I'm driving/receiving the VREFB signals with Tiva MCU. What I see is that the first 2 channels out of 8 are working as expected, the rest are not. Because of the pull up both input and output channels are "high" to the respective voltage, when I drive a low from the controller the first 2 channels drops to about 0.5V and the output are 0.5V respectively. The other 6 channels drops to 3V from 3.3V and stay high at the output. This is done one channel at a time.

Why is this behaving like that?