Other Parts Discussed in Thread: SN74LV08A
I am using the SN74LV08A gate to protect a processor from voltage while not powered.
If there is no voltage on VCC, is it harmful for this part (SN74LV08A) to receive a voltage on one of the inputs? (1A, 2B, 2A, 2B, 3A, 3B, 4A, 4B) The data sheet states that the input voltage range is -.5V to 7V. Does that include when VCC is off too?
Also, if there is no voltage on VCC, is it possible to have any accidental voltage on the outputs (1Y, 2Y, 3Y, 4Y) if a voltage is supplied on the inputs? (1A, 2B, 2A, 2B, 3A, 3B, 4A, 4B)
Thanks