Other Parts Discussed in Thread: LSF0108
Hello,
I would like to ask you a few questions regarding LSF0108:
1. In 10.2.1.2.1 of the datasheet, it talks about outputs A3 and B4 in Fig 6, but there is no A3 and B4 in Fig 6, which figure or which pins in which figure they refer to?
2. In 10.2.1.2.1 of the datasheet, it talks about push-pull or open -drain, please confirm the following: for push-pull, the RL is connected between the output pin and the ground; for open-drain, the RL is between the output and Vpu.
3. Can the FPGA LVCMOS 2.5V output directly connect to the input pin Ax without pull-up, or pull-down?
4. In Fig 9 on page 15 of the datasheet, Vref_B and EN is connected to a power supply, should it be Vpu? OR Vpu = Vref_B =VEN?
5. What is value for the capacitor which connect to EN?
The system is the following:
(FPGA, LVCMOS 2.5V output) -> (voltage translator: LSF0108) -> (50 ohm to ground for impedance match in a coax cable) ->(5V TTL input 54F68).