This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Synchronize 8 logic channels with ~ 2 ns accuracy.

Other Parts Discussed in Thread: SN74ALVTH16373, SN74LVC573A, SN74LVC373A, SN74LVT573, SN74LVC574A, SN74LVC374A, SN74LVT574

Hi there, 

as the subjects states, I have 8 logic channels (called T1:8) coming out of a microcontroller and going into 8 devices (something like DACs), that are clocked synchronously with 180 MHz. The microcontroller is not clocked synchronous to the 8 devices, so T1:8 may change their state at any arbitrary phase position, relative to the device clock. What I need is something like an 8 Bit-Latch, that is clocked by the device clock and fed with T1:8. Can anyone recommend an IC, that fits those needs? I thought about something like the 74AC11373 but I need it much, much faster. The high/low level of the device/latch clock will last for <~2.8 ns. A skew time of less then 2 ns is necessary. 

Thanks in advance! 

Korbi