Hi,
We are using TXB0304 to interface a 3.0 SPI FLASH to a processor which has 1.8V SPI interface. We can recognise the FLASH and perform short read/erase/write cycles. When we are trying to perform erasing/writing large amounts of data we get issues. One of the things we notice in the datasheet for the TXB0304 is the drive requirements which needs to be +/- 3 mA. The CPU that we are using can sink 3mA but cannot source more than 1mA. Can this be an issue? When we check the waveforms on the scope - they look at the right level.
Any clues - pointers which might explain the behaviour. The FLASH device we are using is N25Q512 from Micron.
thanks
regards, Ranjeet