This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Output current for level shifter devices

Guru 19785 points

Other Parts Discussed in Thread: SN74AVC8T245, SN74LVC8T245

Hi Team,

Could you please tell me about the output current which is supported for each device ?

In some devices, I can find the recommended output current range in the datasheet, however, some devices does not have the recommended output current range. In this case, how could I understand the maximum output current ?

There is an output current description in the absolute maximum ratings, however, I believe recommended range would be lower than this specification.

I am looking for a device which could support output current more than 20mA, when level shifting from 1.8V to 3.3V.

Could you give us your advice and recommendation ?

Thanks in advance.

Best Regards,

Kawai

  • Hi  Kawai,

    For translator device, the output current will depend on supply voltage.

    For TXS device, DC current will depend on voltage supply and pull-up resistor. AC current will be about 15mA during low-to-hihg transition and hihg-to-low transition.

    For TXB device, DC current will depend on voltage supply and internal series resistor. AC current will be about 15mA during low-to-hihg transition and hihg-to-low transition.

    For SN74AVC device, please refer to SN74AVC8T245 'Iol' and 'Ioh'.

    For SN74LVC device, please refer to SN74LVC8T245 'Iol' and 'Ioh'.

    Thanks

    Wei