This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
what will be the output at R25 when both inputs are 0V,
This is open drain so i already put an pullup (R24--> 100k and 10K ) i am expecting as 12v at R25 but i am getting only 7V.
is that i am wrong ?or what is the problem here ? please reply me soon anyone
Hi Ryan, thanks .
Before getting your reply( fortunately you too suggested the same:-) ) we did lower the voltage option and completed the testing ,but our need (requirement) is any other IC(device) which can support more output Voltage(such that 12V to 13V range) that will be help for us.
if possible same package .
waiting for your support ..
- Praveen