Hi,
I have read the data sheet of the mentioned item but one thing was not clear for me. It says "This allow for universal low-voltage bidirectional translation between any of the 1.8-V, 2.5-V, 3.3-V and 5.5-V power nodes." , beside this the device can operate with Vcca and Vccb set at 1.65-V to 5.5-V.
The logic levels are described in ranges shown in the following table.
My question is: Does this device suitable for connecting a uC with 2.8 V and an LCD with 5 V power supply or it is only useable for the 1.8-V, 2.5-V, 3.3-V and 5.5-V?