Other Parts Discussed in Thread: PCI2250
Hi,
I have to implement a PCI interface with a Xilinx Spartan-6 FPGA for a legacy product (PCI universal add-in board). As that FPGA is not 5V tolerant, I have to add an interface between it and PCI connector (5V and 3V3 compatible) in order to bidirectionally translate voltage levels.
I think I have two possible solutions:
- On the one hand, the PCI bridge PCI2250. But since I'm going to use it as a simple interface (not as a real bridge, because there's not going to be a secondary PCI bus in the add-in card), I suppose that chip is too much for what I really need.
- On the other hand, SN54CBT16244, wich has a CON lower than 10 pF. But I'm not really sure about whether this option would be appropriate or not (PCI compliant).
Any idea about this? Would the PCI2250 option be the best of all? Or is there any voltage translator or any other chip more suitable for this application?
Thanks in advance
Regards
Jesus