This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Delay IC

Guru 29720 points
Other Parts Discussed in Thread: LM3880

Hi Team,

My customer is looking for "delay IC" as the following.
He would like to have additional delay intensionally.
---------------------------------
Delay time: 1~100ms(fixed value is applicable)
Interface: CMOS
---------------------------------
Is there any device for TI?

Best Regards,
Yaita

  • Hi Yaita,

    if you are looking for a IC that will delay analog signal, then you will not find it anywhere. There was old IC's called bucket brigade. For delaying analog signal you can design all-pass filter. All-pass filter will pass all signal components without degrading its amplitude, but will only delay every component of the signal for the same amount. All-pass filters have constant group delay, and because of that, they are used as delay circuits for analog signal.All-pass filter can be digitally controller if you instead of the fixed resistors put digital potentiometer. When you change resistor value, it will cause change in delay value.

    Delaying digital signal is much more simpler. There are million IC's on the market, or you can use ultra low count MCU.

    Best regards,

    Vojin 

  • It is the delay IC of digital signal.
    Could you let me know the model number of TI device except MCU as a guide?

    Best Regards,
    Yaita

  • yeah its correct..........

  • I found LM3880 for this requirement.
    Thanks.

    Best Regards,
    Yaita