What is the channel-to-channel propagation delay skew of the SN74AVC32T245ZKER?
Using operating conditions:
- VCCA 3.3V
- VCCB 2.5V
- Data rate 125Mbps
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the channel-to-channel propagation delay skew of the SN74AVC32T245ZKER?
Using operating conditions:
Hi,
If data is tranlated from 3.3V to 2.5V, SN74AVC32T245 cannot support 250Mbps data rate. If data is tranlated from 2.5V to 3.3V, please run some simulation with IBIS model since propagation delay will depend on output loads. In out datasheet, tplh is measured under typical load circuits which show on page 13 in the datasheet.
Thanks
We only need 125 Mbps so this is fine.
However the actual question is: how much is the propagation delay / skew between two channels in the same device with the same load? (eg channel to channel skew)
Hi Guido,
Becasue we didn't test channel-to-channel time skew in tranlstor portfolio. It is better to run some simulation with IBIS model to make sure our chip performance.
Thanks