This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ttl logic. need to drive pins high and low. ic? pcm4202

Other Parts Discussed in Thread: PCM4202

Hi everyone. Here is a noob question. From a person with minimal background in electronics. I have an ADC pcm4202 I would like to use in in H/W control mode.

There are come pins that I need to have set high or low using TTL logic.  2.52V-3.6V High and 0V-1.08V Low. Could you suggest which IC chip I can use to accomplish this task. Also, one that would have not to many pins and easy to use for a noob.

thank you,

Konstantin M 

  • Hi Konstantin,

    Can you tell me more about your application?  If you have a schematic or functional diagram, it would be very helpful.

    If you are just looking to hold a pin high or low, a pull-up or pull-down resistor (10k is usually a good value) would work fine.  Perhaps once I understand what you are trying to do, I will be able to help you further.