This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

74HC165 at 3.3V

Hi all,

I'm going to be using this parallel-to-serial shift register at 3.3V, and I see it's not been characterized at this voltage in the datasheet (www.ti.com/.../sn74hc165.pdf).

I'm most interested in knowing the TIMING CHARACTERISTICS and the SWITCHING CHARACTERISTIC on pages 6 and 7. Is this data available, either directly or as a recommendation/guess based on the 2V and 4.5V data?

Thanks!

  • The recommended method for finding values between those listed on the datasheet is linear interpolation.  I have found that Excel is great for quickly doing conversions of these values if you need a lot done in a short time.  The image below shows an example of how I usually do this.  If I can provide any other help, please let me know. 

     

  • Hi Emrys,

    The behavior is obviously non-linear based on the 2V, 4.5V, and 6V curves. It's more like a log curve where as Vcc continues to increase the change in value goes down. So do you recommend linear interpolation because it will give a lower bound to the actual value at some intermediate voltage?
  • Evan,

    You are correct that this is non-linear, but the reason we give 3 values on the datasheet is to allow linear approximation.  There is also some guard-banding involved to ensure that the values given are achievable (this is true for basically everything on any of our datasheets).