This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[ TXS0206 ] For eMMC

Other Parts Discussed in Thread: TXS0206, TXS0206-1, TXS0108E

[ TXS0206 ] For eMMC

Hi,

My customer has been studying to use two pcs of TXS0206 for the connection between their CPU and eMMC.

Here is the idea how CPU and eMMC are connected via TXS0206.

  • TXS0206-1: use all of DATAnA/B, CMDA/B and CLKA/B
  • TXS0206-2: use all of DATAnA/B
  • VCCA (CPU): 3.3V (or 1.8V)
  • VCCB (eMMC): 1.8V
  • For both devices, CLK-f is not used, so left open

Do you think there are any concerns to be considered?

What I'm concerned are...

Q1: On TXS0206-2, CMDA/B and CLKA/B are left open

Can these CMDA/B and CLKA/B be left open?

Q2: For some cases, VCCA and VCCB are getting same 1.8V. 

Since datasheet has some specification for the case of VCCA and VCCB are same voltage, this should be okay.

Thank you for your support in advance. Please let me know, if I miss some information.

Thanks,

Ken

 

Other reference: 

TXS0206 or TXS0108E for eMMC

https://e2e.ti.com/support/interface/etc_interface/f/391/p/343093/1199027#1199027