This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC244A supports DC input

Other Parts Discussed in Thread: SN74LVC244A

HI,

This is a buffer and it does not state clearly in the datasheet. Does SN74LVC244A support a DC input(0 Hz)?

Thanks.

  • Di Wang,
    Yes. All logic gates support DC inputs. An input above the specified VIH level is considered a logical "HIGH" input, and an input below the VIL level is considered a "LOW" input. The inputs to the logic gate must remain within the specifications listed in the Recommended Operating Conditions table in the datasheet.