Other Parts Discussed in Thread: CD74HC164, SN74LV164A, SN74LVC2G132
Hello
Is there a low power version of the 74AC164 available.
Thank you
Gary
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CD74HC164, SN74LV164A, SN74LVC2G132
Hello
Is there a low power version of the 74AC164 available.
Thank you
Gary
Hello Gary ,
There are numerous choices for lower power shift registers at TI . I can give couple of suggestions here below :
CD74HC164 has 80uA Max Icc consumption .
SN74LV164A has 20uA Max Icc consumption .
http://www.ti.com/product/CD74AC164/compare# . Using this link , you can select appropriate devices suitable for your application based on various input criteria .
Please let me know if this helps .
On power up, what are the states of the outputs?
I can send a tina model of my design.
Thanks
Gary
"The #5 output will go thur and inverter to the MR_ to clear and restart the sequence."
Gary,
I'm not entirely sure what you mean in the above statement -- can you post a schematic?
The following circuit should start all outputs low and allow the feedback loop you wanted:
I have configured the SN74LVC2G132 above into a 'AND' gate -- I drew both NAND gates for clarity of the design.
When Vcc is turned on, the gates will all be powered on, but the input to A will be much slower than the others. The output to CLR\ will be zero when the system is turned on because A is zero -- regardless of the B value, the CLR\ line will be forced low until A goes high. Once A is high, B will control the CLR\ output -- when B is low, CLR\ is high, and when B is high, CLR\ is low.
Note that I have selected a device with Schmitt-trigger inputs because the RC input will be very slow and could cause problems if a Schmitt-trigger is not used.
I am using a momentary switch on the Clock in. Do I need to debounce this input?
Thank you
Gary
I have everything working, thanks.
Currently I have 100 ohm resistors between the shift register outputs and the SOT-23 N Fets.
Do I need a damping resistor or can i drive the N Fets directly?
Thank you
Gary