Other Parts Discussed in Thread: SN74ALVC164245
The SN74ALVC164245 has high output drive of 24MA.
Need same device with lower output current and same 5V output logic
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN74ALVC164245
The SN74ALVC164245 has high output drive of 24MA.
Need same device with lower output current and same 5V output logic
Eli,
The SN74ALVC164245 can take a 3.3-V input on the "A" side and output a 5-V signal on the "B" side. Were you looking for different functionality?
Also, 24 mA is the maximum current a single channel can output. This current is dependent on Ohm's law for the load and the output voltage. The device will only output this current if the load on one of the pins is 5/.024 = 208 Ohms. Is there a reason you want a device with lower output drive?