This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4504B for 3.3V to 15V level translation

Other Parts Discussed in Thread: CD4504B, TMS320F28335

I'm planning on using the CD4504B part to level translate from 3.3V to 15V.

The inputs to the CD4504B come from a '28335 DSP (3.3V).

Vcc for the CD4504B will be 5V.  Vdd for the CD4504B will be 15V.  CD4504B will be in TTL-CMOS mode.

The specs on the '28335 outputs and the CD4504B inputs look like there should be no issue.

Two questions:

1.  Is there a better part available to accomplish 3.3V to 15V level translation?

2.  Is there an issue or limitation with the CD4504B in this application that I am not aware of?

Thanks,

Chris