Other Parts Discussed in Thread: SN74LV08A
We are currently using the SN74LV08A with the following:
Vcc = 3.3V
1A (pin 1) = 3.3V
Can 1B (pin 2) safely be exposed to 5V given the above conditions?
If 1B is at 5V, will the output 1Y (pin 3) be 3.3V?
Thanks