Other Parts Discussed in Thread: CD4053B
Hi Team,
In CD4053B datasheet p.9,
what does any channel mean?
what difference between common out/in and any channel?
both data are difference.
Thank you in advance!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jason ,
The COM channel refers to the common channel or the input port and any channel would refer to A or /A channels as shown here below :
This was meant to be like a common statement encompassing the other 2 devices of the family which explicitly state the COM channel . It is little different in the case of CD4053B though.
Hi sir,
Thank you for your reply, but I still don't understand.
Any channel mean the BW of all channel is 60db, but common channel mean only one channel. Am I right?
in addition, customer want to ask the condition below if it is workable.
1. Send 5-10MHz signal via CD4053B
2. The amplitude of this signal is around 4V
3. channel to channel switching frequency is 10kHz
4. VDD (V)=5V. (I think VDD should be 10V)
thank you in advance!!
BR,
Jason
Hi Jason ,
Common channel means channel at which input is sent and other channel will be the output . CD4051 has 1 COM channel , CD4052 has 2 COM channels , CD4053 has 3 COM channels .
1) Yes , CD4053B can handle 5-10MHz at 4V with the Vdd you specified .
What do you mean by channel to channel switching frequency ?