Hi,
For SN74LVCH8T245 We do not use ALL the the A Inputs and B Outputs, What are we need to do with them ? Connect the A inputs to GND ?
Thanks,
Doron
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
For SN74LVCH8T245 We do not use ALL the the A Inputs and B Outputs, What are we need to do with them ? Connect the A inputs to GND ?
Thanks,
Doron
Hi Doron
If you are using SN74LVC8T245 (non "H" version), please follow Fancis recommendation and tie the unused inputs to GND. It is recommend to pull down through a 1K resistor.
If you are using SN74LVCH8T245, as your title says, do not use pull-ups or pull down. These parts have bus-hold circuitry. As stated on page 2 of the datasheet "
"Active bus-hold circuitry holds unused or undriven inputs at a valid logic state. Use of pullup or pulldown resistors with the bus-hold circuitry is not recommended."
Generally, pullup and pulldown resistors should not be used on the inputs of devices with bus hold. In applications that require pullup or pulldown resistors to hold the inputs at a specific logic level, the bus-hold current maximum specification should be considered.
The resistor value should be chosen to overcome bus hold under worst-case conditions. The resistor must supply enough current so that the input is pulled through the threshold to the desired logic level. If the current supplied is too weak, the input node could be held near the threshold, causing a high ICC that could damage the part.
Hope this helps.
Thanks