Other Parts Discussed in Thread: TXB0304, TXB0108
What is the differences between TXB0304 and TXB0108 beside the number of ports?
I have a CPU that has 1.8V IO for memory interface, the NOR flash are 1.8V IO and the SRAM and NAND are 3.3V IO. Can I use just one TXB0108 to interface the 1.8V side to the CPU and NOR and the 3.3V side to the SRAM and NAND?