We are facing problem with the IC SN74LVCC3245APWR (Octal Transceiver)
VCCA=3.3V; Decoupling Capacitor - 0.1uF VCCB=5V; Decoupling Capacitor - 0.1uF DIR=3.3V with 4.7K ohm Pull up resistor OE#=GND with 4.7K ohm Pull down resistor Temp : Ambient 30 deg C.
Input pins was controlled by FPGA and '0' is driven by default. B port pins have 1Kohm pull down resistor.
B port pins were connected to SN74HCT14D (Inverter) through 26AWG cable.
B port pins were connected to SN74HCT14D through a cable of 26AWG.
Output pins were not toggling as per the input voltage. B port pins were showing 0 ohms with respect to ground.
Please guide us.