Other Parts Discussed in Thread: SN74AVC32T245
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN74AVC32T245
Hi Shreyas-san,
Thank you for moving my post.
I am looking forward to hearing from your colleague.
Best regards,
Kato
Hi Francis-san,
Thank you for your quick response.
Is my understanding correct although I understood that SN74AVC32T245 supports 1.8V to 3.3V Level-Shifting at 380Mbps(clock:380MHz, data:190MHz) and 3.3V to 1.8V Translation at 200Mbps(clock:200MHz, data:100MHz) ?
Our customer can use SN74AVC32T245 if it is correct.
So, would you suggest other proper soultions if you have the smaller package size ?
Could you please give me your advice about it ?
Best regards,
Kato
Hi Francis-san,
Thank you for your advice.
I understood that the maximum data rate is more than 200Mbps(the level-shifting:380Mbps, the translation:200Mbps) if VCCA and VCCB are more than 1.8V.
So, I have two questions.
Is the maximum data rate equal for both A-port to B-port and B-port to A-port if the power supply voltage for VCCA and VCCB is equal although the delay time is different between A-port to B-port and B-port to A-port ?
In addition, could you please tell me the maximum load capacitance to satisfy the maximum data rate(380Mbps@1.8V and 200Mbps@1.8V) for the output terminals?
Best regards,
Kato