Other Parts Discussed in Thread: LSF0108
Hello!
The datasheet of LSF0108 does not specify if it can be used with VrefA = VrefB.
I want to use it as a buffer because of the high output current. I want to drive ~25pF load with 60MHz, but I need no level translation.
Is it reliable to drive both voltage sides with the same level? 3.3V for this instance.