Other Parts Discussed in Thread: SN74LVC541A
Hi
I'm using an SN74LVC541A to drop some normally 5V signals down to 3.3V (VCC for the device). the datasheet says this is OK.
My problem is that my signal source could under a single fault condition rise up to 24V.
The data sheet has a note in section 7.1 (absolute maximum ratings) which reads "(2) The input negative-voltage and output voltage ratings may be exceeded if the input and output current ratings are observed."
I had originally mis-read this statement as applying tom both negative and positive voltage ratings. But it only applies to input voltages less than 0V, What about voltages greater than the 6.5V maximum rating.
I've got lots of resistance in series with the input such that if the fault occurred the current into the device would be no more than about 40uA.
Would this damage the device.
Thanks