Customer would like to use LSF0108 to perform Low voltage to high voltage level shifter(ie 3.3V to 5V). the results is showing the output can not up to 5V. please help review the test circuit and results then supporting this application.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Customer would like to use LSF0108 to perform Low voltage to high voltage level shifter(ie 3.3V to 5V). the results is showing the output can not up to 5V. please help review the test circuit and results then supporting this application.
Hi Peter ,
I do not see the pull up resistor at the B8 output . The pullup resistor needs to be connected to 5V .
The LSF is a passive switch which does the translation by having external pullup resistor pulling the output to the desired voltage level when the switch is off . when the A signal is low , the switch is on , thereby having B at the same level .
The driver at the A side must be able to handle the current flowing through the pullup resistor and the small ron of the LSF switch itself when in low state (refer to the IOL of A side driver) .
I will also attach an app report and EVM user guide which will be very helpful in understanding the device and your application design too .