We are looking at using the TXS0206 or TXS02612 in a 1.8V CPU <-> 3.3V SDcard translation.
I do not have access to the complete SD card specifications, but I have found the datasheets for a few SD cards and they all seem to agree.
Voh @100uA = .75* VCC = 2.475V
Vol @ 100uA = .125 * VCC = .4125V
The TXS0206 has the following input requirements on the B inputs.
Vih = VCC - .2V = 3.1V
Vil = .15V
From the above it appears that SD cards will not be able to trigger logic high and low on the B inputs of the TXS0206. Since this chip is designed specifically for use with SD cards I feel that I am missing something in the operation of the part.
Can you describe how the SD card outputs can meet the require logic thresholds of the TXS0206?