Other Parts Discussed in Thread: TXS0108E, MSP430F5244
I need to isolate my UART to USB bridge chip (FTID FT232RQ) from my MSP430F5244 so that power does not back feed in my circuit and cause the device to not shut down. I have 65 lines that power could inadvertently be transferred through. Can I use the TXS0108E to solve this issue? I would drive VCCb (3.3VDC) from the processor side, and VCCa (3.3VDC) from the USB. The OE pin would also be driven from USB side. So if the device is on and not connected to the USB, no communications should occur and no power should be transferred the FTDI chip. When the USB is plugged in, the FTDI chip is powered, and the TSX0108E will turn VCCa and OE on allowing communications.
Will this work or is there another device i should use.
Thanks.