Other Parts Discussed in Thread: TXB0106
Hi
What is the drive strength of TXB0106?
Can you please specify the max Ioh and Iol level supported by the device?
Thanks in advance
Regards
Sushruta
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TXB0106
Hi
What is the drive strength of TXB0106?
Can you please specify the max Ioh and Iol level supported by the device?
Thanks in advance
Regards
Sushruta
Hello Sushruta,
An auto direction sensing translator will have a weaker drive strength. This is due to the requirements in order to make it auto direction sensing. If the driver is too strong, the device connected won't be able to over come the drive strength to force its own signal onto the bus. The translators look for their drive strength being overcome by a device and use that to detect which side is propagating to the other.
However, our TXS series offers rise time accelerators to make it behave like it has a stronger drive strength, while the static drive strength is much lower (~1mA) and allows for the part to be used as an I2C translator.
We do not have a TXS0106, but we do have a TXS0108, which features edge accelerators for both rising and falling.
I'm not sure what interface you're using this for, or what speeds you're looking at.
Hello Jonathan
We are using TXB0106 in between Xilinx FPGA Zynq IO pins and external interface.
I understand that for proper operation, the device driving the data I/Os of the TXB0106 must have drive strength of at least ±2 mA.
I wanted to know if TXB0106 will be able to drive FPGA IOs when above condition is met?
Thanks and Regards
Sushruta
Thanks for the information provided.
Does this mean, if the current of the input signal is more than 2mA (which is guaranteed in our case), the device will simply pass the input signal to output port?
Regards
Sushruta