Other Parts Discussed in Thread: CD4504B
Hi,
According the datasheet, all inputs of the CD4504B are protected by an CMOS protection network, which is not further specified.
Is this CMOS protection network adequate for ESD events of 15K, or do I need to add additional ESD suppressors?
For example, the TPD4E004DRYR. Which immediately raises another question.
In my case, Vcc is 3.3 V and according the datasheet the absolute maximum input voltage is Vcc + 0.5 V.
The breakdown voltage of the TPD4E004DRYR is 6 V. Is this OK, or is the breakdown voltage to high (> 3.3 + 0.5)?
I would expect that the inputs of CD4504B would survive at least 20V.
Thanks.