Hi
We have used TXB0106 IC in our design.
Though we do not need bi-directional translation, we are using this IC for BoM cost optimization.
We have used TXB0106 IC in between HCPL-6651 optocoupler and Zynq SoC.
TXB0106 IC translates output from optocoupler to Zynq SoC inputs. Hence, it always operates in one direction only.
The output of optocoupler is an open collector pin. Hence, this signal is pulled up to 5V.
I wanted to know if there are any constraints for choosing pull up resistor?
It is given in datasheet that "For proper operation, the device driving the data I/Os of the TXB0106 must have drive strength of at least ±2 mA". So, is it ok if I use 2K resistor?
Awaiting for your reply.
Thanks and Regards
Sushruta