Other Parts Discussed in Thread: PCF8575, PCA9555, PCA9539, PCA9535
Dear TI Support,
We are using the PCF8575 IO expander (Vcc = 5.0V)
Toggling output ports works ok when there is no load, but when connecting output load of (0.6mA - 0.8mA) the "high" output level reaches ~1.5V instead of 5V.
Unfortunately, in the datasheet the IOL is specified for VOL of 0.4V and 1.0V only.
We expect this part to operate as push-pull output 0V to 5.0V, directly connected to the described load, without additional external devices.
Please advice.
Thanks,
Igal