This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCB surface mount configurable Logic



Greetings. Can anyone tell me whether there is a component available that will combine a voltage comparator with a a NOR gate. I'm looking for the output from the voltage comparator to be one of the inputs into the NOR gate with the other input held low. 1-5vdc and the voltages with both be in the range 0-750mV

Thanks in advance

  • Hi Brendan ,

    it is unlikely that there would be a integrated solution with comparator and NOR gate in a single package . The output desired is 0 to 0.75V ? The high voltage is again unlikely in our portfolio.
    The AUC1G02 is NOR gate which goes down to 0.8V Vcc min which is the lowest on offer . There are numerous small package offerings available both in logic and comparators which could be considered .They may be smaller than the combined single package area in some cases .