Other Parts Discussed in Thread: TXB0108
I would like to use two TXB0108 in series. I am not sure if this will be a problem to decide the direction of the signals...
The idea is to use one TXB0108 in a board to convert from 5V to 3.3V and on another board attached to the previous one another TXB0108 supplied with 3.3V in both sides. The idea is that the second TXB0108 will be only to protect the FPGA which is connected to it.
Maybe there is a more elegant way to protect the FPGA? Protecting means that if someone plugs something wrong the the TXB0108 will burn and not the FPGA...