This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High Frequency Square Wave Division Duty Cycle Adjust

Other Parts Discussed in Thread: SN74LS292, SN74ACT74

Hello to all,   My name is Ken and I am a first time poster and terrible typer so I apologize for that.

My project is as follows, Sine wave input 30mhz / Square Wave Output  30mhz or 60mhz depending on choice for frequency division or not to achieve a dual output 30mhz per output with duty cycle adjustments on each output.  I was looking at using a pair of 74act74 devices to divide my 60mhz trigger and provide my duty cycle adjustments.

I am currently using LtSpice which is all I have. The devices from LT have got me to the 60mhz clock output and now my question is what device from TI, D flip flop or otherwise would be a good choice from here. Any Help is appreciated.

Ken

  • Hi Ken ,

    A conversion from sine wave to square wave would require a Schmitt trigger which can tolerate slow rising edge signals and trigger the device at the threshold point to generate a square wave . Also ,using a D flip flop with input frequency at 60Mhz and having the Q\ output tied back to its D input would result in output frequency of 30Mhz . further division is possible with cascading the flipflops.
  • Hi Ken,

    Apart from using the D flipflops, you can also look into using the SN74LS292/4 programmable freq dividers and timers.
  • Hi Shreyas,

    Thank you for the reply, at this time using Ltspice and components within LT I have my conversion and doubling completed.
    my main concern at the 60mhz clock input using a SN74ACT74N would be sufficient at that frequency.
    Looking at the datasheet it is questionable. Do you have a recommendation otherwise? Only adding to the project complexity it must be frequency agile and duty cycle adjustable the duty cycle adjustments I have already figured out using 2 SN74ACT74N Flip Flops but have no way of testing them in Ltspice can you help me there I have no model and i am a new user of Ltspice and conversions are difficult. Thank You again and I will look at the SN74LS292?4 datasheet

    Ken
  • Going by the frequency spec , the SN74ACT74 should be able to handle 60Mhz well .The max clock frequency is around 125Mhz . There are other flip flops with higher frequency ratings . I have filtered them here .