I've attached the datasheet of schematic of logic level shifter pcb. I need to connect 3.3V compatible pins of RPi to 5V compatible pins of some other sensor.
As shown in the circuit of the datsheet on page no. 5, I connect 3.3V to VCCA, 5V to VCCB, GND to OE, RPi pin to any of AX. I expect 5V pin on corresponding BX pin when 3.3V is applied to AX pin. Instead there is 0V on it.  6761.level.pdf