This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC540 Logic Level details



Hi,

I am SN74LVC540APW device in my design and proto-boards testing are in progress.

 The schematic is attached and the inverter IC pin connection details are below.

  • OE1*(pin1) & OE2*(pin19) tied to ground permanently.
  • Input pins are connected to Artix-7series FPGA device output.
  • When FPGA is not configured state, FPGA outputs are in tri-state.
  • In this case, what is output of SN74LVC540APW device?
  • In datasheet, there is no information for this condition

Issue:

  • We have 5-protoboards. In that I am seeing the difference in inverter behavior.
  • Case1: In board01, if the inputs are tri-state(low-measured using Oscilloscope) and the outputs are Low
  • Case2: In board02, if the inputs are tri-state(Low) and the outputs are high

Please let me know why the difference is happening and what is the cause for this problem?

Note: Part marking of the Devices are same.

Thanks,

Jeyalakshmi