This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am decreasing the duty cycle of TTL input signal (100kHz, duty cycle 50%) to 10%. The input signal was generated using a function generater(Stanford Research System, DS345). According to the datasheet of SN74121, there should be no jittering on the output signal (jitter free operation up to 90%).
However, I found out that the output show about 5ns jitter on the rising edge and the falling edge.
Can anyone explain why this is happening?