Dear TI Community,
I'm using SN74LVC16T245 for translating level from 2.8V to 3.3V.
Port A is connected to 2.8V and which is input (camera I/O signal connected).
Port B is connected to 3.3V and which is output (connected to processor).
When we suspend the camera, then nothing will be feed into the port A of SN74LVC16T245. This time what will be the I/O level state of Port B ?
In other words, If the input of Port A is not valid state, then what will be the logic level state of Port B ?
Regards,
Azlum