This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0108 datasheet layout section OE pin

Other Parts Discussed in Thread: TXB0108

Hi,

In TXB0108 datasheet, the layout example(section11.2). OE pin is not connected to any IO pin.

I think it is wrong. Is it should be connected with a control signal to pull OE pin to high?

Thanks

  • Daniel,

    Thank you for your feedback. I tend to agree.

    There is a note below the pin that implies OE should be driven high once both power rails are stable. However, a layout that illustrates a connection to a GPIO pin would be better. Just looking at the illustation, it looks as if the TXB0108 is permanently disabled.

    I will submit a request to modify the datasheet accordingly. Thank you.

    Best Regards,
    Nirav