Hello,
I am looking for the information regarding SN7406N through hole component:
1. is it halogen free?
2. what is the max temp and up to what time it can go on wave soldering machine?
3. what is the max temp and up to what time it can go on manual soldering?
4. is it water sensitive component?
5. what type of reliability has done with respect to thermal shock or thermal cycling?
Thanks,
Milan Shah
978-392-5577 office
585-503-3252 cell