I'm looking for thermal data for the following
SN74LVC1G74DQER
I need:
Theta JB
Theta JC
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm looking for thermal data for the following
SN74LVC1G74DQER
I need:
Theta JB
Theta JC
thanks
Eric,
I apologize for leaving that out. It is degrees Celsius per Watt or
°C/W
Respectfully,
Cameron
Eric,
If your supply voltage is from 0.8 - 3.6V then you could use the SN74AUP1G74 which has
|
Theta JC |
108.1°C/W |
|
Theta JB |
120.3 °C/W |
Otherwise, I am submitting a request for the thermal data of the other packages.
Thank you,
Cameron
*Edit SN74AUP1G74 Range from 0.8-3.6V
Eric,
The SN74LVC1G74DCTR has better thermal performance of
|
Theta JC |
117.8°C/W |
|
Theta JB |
100.7°C/W |
This is the SM8 (or DCT) package.
I hope this works better.
Thank you,
Cameron