The spec describes a Icc
VI = GND or (VCC to 3.6 V), ICC 0.8 V to 3.6 V 0.5 0.9 μA
and then something called delta Iccc
ΔICC VI = VCC – 0.6 V (1) , IO = 0 3.3 V 40 50 μA
What is this? I would like to create a nearly zero power low freq clock signal, but this part I cant understad what it is or even what condition they are defining.
Shall I understand that as long as the Vi is at VCC or ground then you get <1u but if you sag to .6V under VCC the you start to dway power? That would make some sence though they did not make the same condition for a grounded Vi with some small offett
Is there any way to predict the dynamic current draw?