Other Parts Discussed in Thread: SN74LVC374A
can we use 74/54LVC16244 with 16MHz clock ? What’s the maximum speed it can work?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN74LVC374A
can we use 74/54LVC16244 with 16MHz clock ? What’s the maximum speed it can work?
Hi eli,
The short answer is: Yes, SN74LVC16244 will operate with a 16MHz signal.
The best way to estimate the maximum speed of a logic device is to find a clocked device in the same family. In this case, SN74LVC374A is a D-Type flip flop that operates on the same technology as SN74LVC16244 (both from the LVC logic family), and that flip-flop can operate up to 100 MHz. Since a flip-flop is far more complex than a buffer, you can be sure that the maximum frequency for the buffer will be significantly higher (and thus using the same value for fmax is safe).
This is actually in our FAQ - you can read a bit more here.