This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVCH16T245 current consumption

Expert 1780 points

 Hello,

          In our board FPGA I/O lines are connected to the inputs of the 245 and the I/O voltage is set to 2.5V. The FPGA is not configured so I presume the interface pins between the FPGA and 245 must be tri-stated. The 245 might either be pulling up its inputs (inputs are at VREFA of 2.5V). The device is consuming a lot of  current  and getting heated up (up to 2.5W). Please advise. 

Port A is referenced to 2.5V and Port B to 5V. The level translation is from A to B.

  • SM,

    Sorry for the delayed response. I was on vacation.

    1. I would suggest that you double check if the FPGA really does tri-state the pins instead of assuming.
    2. Do you have a schematic that you can share with us?

    Best Regards,
    Nirav
  • Nirav,

           Thank you for your reply.

    1) I got it confirmed today. The outputs of the FPGA are tri-stated. 

    2) I'll try to get the schematic. 

    Regards,

    SM>

  • Nirav,

     An observation:

    If OE is disconnected from GND and the inputs are not tri-state then the current consumption becomes normal.
    & 
    If OE is connected to GND and inputs are not tri-state then the current consumption is high.