This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV541A SN package total width

Other Parts Discussed in Thread: SN74LV541A

I am curious what is the maximum extension from pin edge to pin edge of the SN (soic-20) package on the SN74LV541A?  Datasheet says it is ~7.8mm but this is very odd, as I have only seen soic packages that either 6 or 12 mm if they are thin or wide body. Can anyone confirm the values from the datasheet?