Hi,
This an extract of the electrical characteristics table of SN74LVC1T45 :
Is the data surrounded in red rectangular concerns only the DIR pin ? If yes, what is the input leakage current for ports A and B ?
Thank you in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
This an extract of the electrical characteristics table of SN74LVC1T45 :
Is the data surrounded in red rectangular concerns only the DIR pin ? If yes, what is the input leakage current for ports A and B ?
Thank you in advance.
AIT,
AIT GHRIB Abderrahman said:Is the data surrounded in red rectangular concerns only the DIR pin?
Yes that is correct.
AIT GHRIB Abderrahman said:What is the input leakage current for ports A and B ?
I will get back to you on this.
Best Regards,
Nirav
AIT,
Lab measurements are provided below. Leakage is much less than 1 uA for both pin A (when configured as an input with DIR pin = High) and pin B (when configured as an input with DIR pin = Low).
My tests included IIH (Pin Leakage when configured to Logic High = VCC) and IIL (Pin Leakage when configured Logic Low = GND)
Keep in mind the data below was collected on one unit and nominal operating temperature. Since this parameter is not specified in the datasheet, there is no characterization data that fully covers your request. However, I would not expect this measurement to significantly vary over PVT.
Best Regards,
Nirav